While tea growing has enjoyed a long history in China, the new generation of tea farmers finds it a tough task to carry on their family legacy in traditional ways. Deng is a millennial farmer who has taken over his family’s 3.3-hectare tea plantation, situated at 1100 meters above sea level in Mengding Mountain near Ya’an City, Sichuan Province in Southwest China.

Deng has encountered the following problems:
- low planting density, with high management cost
- uneven budding, with a low yield
- difficulty in demonstrating the tea’s organic environment in the high mountains, thus making it difficult to get a good price or recognition for his brand, YI YE SHENG.

To tackle these problems, Deng was willing to embrace smart farming technology. He was immediately an ideal candidate when we began searching for a pilot farm to test Seeed’s SenseCAP, the wireless IoT sensor network solution. The smart agriculture solution, which is wittily named “IoTea” for this pilot tea project, was deployed in Deng’s plantation in the high-altitude Mengding Mountain in 2018.

From 2018 to 2022, our SenseCAP devices are widely deployed in various projects. In 2022, we developed the brand-new LoRaWAN wireless S210x Series. Based on the first-Gen industrial sensors, we intend to continuously empower tea farmers without technological background and provide more advantages to our SenseCAP S210x like:
- friendly user experience
- low deployment cost
- low-maintenance cost
- long battery life

The IoT application consists of LR gateways and sensor nodes:
- SenseCAP Wireless Gateway – LoRaWAN
- SenseCAP Wireless Air Temperature and Humidity Sensor – LoRaWAN
- SenseCAP Wireless Barometric Pressure Sensor – LoRaWAN
- SenseCAP Wireless Light Intensity Sensor – LoRaWAN
- SenseCAP LoRaWAN CO2, Temperature, and Humidity Sensor
- SenseCAP Wireless Soil Moisture and Temperature Sensor – LoRaWAN
Note: We have updated the URL to our latest LoRaWAN sensors in SenseCAP S210x series.

With the solution deployed in the tea plantation, Deng is able to monitor the following environmental data which are crucial to tea quality. Among these data, air humidity, temperature, and atmospheric pressure are the main parameters proving the tea’s high-mountain environment.
- Air Temperature
- Air Humidity
- Barometric Pressure
- Light Intensity
- CO2
- Soil Moisture
- Soil Temperature

The environmental data collected provides insights for Deng to manage the farm more efficiently, and with lower labor costs.
More importantly, the historical and real-time environmental data of the farm where their tea is from is made available to end customers, who simply scan the QR code on the tea’s packaging to access the webpage containing the data in graphs. Thus, the tea-growing environment is traceable by the customers, proving the green tea they are enjoying is in fact from the high mountains.
In this way, Deng can gradually build up his brand with loyal customers, and supply to end-users directly with a better price, instead of only selling to large tea companies who dominate the market.

This project also helps contribute to the following Sustainable Development Goals.

About High-mountain Tea
High-mountain tea refers to teas grown in high mountains that are higher than 1000 meters above sea level. Due to the large temperature difference between night and day, the high air humidity and the thick mist, the teas grown in this environment usually contain a higher chlorophyll and amino acids in the tea leaves, which are responsible for the tea quality including its color and taste. The high-mountain tea leaves feature thickness in texture, fresh green in color, and density in trichomes, resulting in rich milky flavors and pleasant floral aromas.
Partners: Yi Ye Sheng

Update April 2020
Here are some photos taken at the tea plantation in late March. And you can see the weatherbeaten SenseCAP still works like a charm after being deployed at Mr. Deng’s tea plantation at Mengding Mountain (1000meters above sea level) for almost 2 years!








What is SenseCAP?
Among the first launch of Seeed IIoT product series, SenseCAP is focusing on wireless environmental sensing applications: smart agriculture, precision farming, and smart city, to name a few. It consists of hardware products (sensors, data-loggers & gateways, etc.), software services (SenseCAP portal, mobile App, open dashboard), and API for device & data management.
About S210X Series
With the IP66 rating, -40 ~ +85C ° operating temperature and built-in 19Ah high-capacity battery, combined with the devices’ low power consumption, the S210X series can operate in harsh outdoor
environments for up to 10 years with a range of up to 10km. The built-in Bluetooth facilitates setup and greatly reduces large-scale deployment costs. Users can focus on application development with the easy set-up, and start retrieving data in a few steps. Just install the device, bind it using the QR code and configure the network, then data can be viewed from the SenseCAP portal, which supports popular IoT protocols such as HTTP and MQTT.
Update June 2022: SenseCAP S210x Series are currently available for purchase. If you have any questions, feel free to leave a comment here, email us ([email protected]), or join the discussion at Discord.
More User Cases
- SenseCAP Deployed in Outdoor Triticale Farm, Empowering Precision Agriculture in Dingzhou, Hebei Province, Northern China
- Smart Agriculture Demonstration Park of Sweet Melons Empowered by SenseCAP in Beihai Guangxi, Southern China
- SenseCAP Empowers Tourism in Hakka Villages by Collecting Environmental Data at in Heyuan, Guangdong, Southern China
- SenseCAP Monitoring Environmental Data in Smart Greenhouses Growing Tropical Fruits in Shandong, Northern China.
- SenseCAP Deployed in Environmental Monitoring Projects in Stockholm, Sweden